How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Multifuse® Products – What They Are
The Bourns® Multifuse® family of Polymeric Positive Temperature Coefficient (PPTC) Resettable Fuses are used in a wide variety of circuit protection applications. Under fault conditions the device resistance will rise exponentially and remain in a “tripped” state, providing continuous circuit protection until the fault is removed. Once the fault is removed, the power cycled through the device will return to its normal low resistance state.
Multifuse® Products – How They Work
Resettable fuses are manufactured in the form of a conductive plastic, which is comprised of a non-conductive crystalline polymer with highly conductive carbon black particles impregnated throughout the crystal lattice. Because of the close proximity of the carbon black particles within the crystal lattice, under normal conditions current is allowed to flow easily through the conductive plastic. However, under a fault condition when there is an increase in current, the conductive plastic heats at the rate of I2R. As the material continues to heat, it eventually reaches the phase transformation temperature, which changes the crystal structure into an amorphous structure. Once the material has transformed into this amorphous structure, the conductive particles become isolated and are unable to conduct current hence the drastic change in material resistance. It is only when the current is removed that the material is allowed to cool and return to its original crystal structure.
Multifuse® Products – How They Are Used
It is the materials used in resettable fuses that allow them to reset after a fault condition has been removed. Resettable fuses exhibit a positive temperature coefficient effect when heated. While many materials exhibit a PTC effect when heated (an increase in resistance in response to a positive change in temperature), what makes the material used in resettable fuses unique is the fact that the increase in resistance changes exponentially rather than in a linear manner. It is because of this transformation from a low resistance state to a high resistance state that allows the resettable fuse to protect loads. It is this transition from the low resistance state to high resistance state that is referred to as tripping. The time it takes for a resettable fuse to trip is relatively quick, depending on how high the fault current is and it can be as quick as a fraction of a second. Hence they are an excellent form of protection for most applications where sensitive devices need extra protection.
Bourns® Automotive Multifuse® Products
As the number of electronic safety, comfort control, and power management systems has increased, the need for integrated reliable circuit protection solutions has evolved into a critical design feature on all new automotive platforms. Bourns has developed its line of Multifuse® Polymeric PTC (PPTC) Resettable Fuses to help automotive manufacturers and designers meet this need. Typical examples of automotive electronic circuits in which Bourns® Multifuse® products are used include:
Resettable Overcurrent Protection
Resettable overcurrent protection offers greater reliability, longer part life and Multifuse® Polymeric PTC Resettable Fuses can be located close to the load being protected instead of traditionally locating fuses in a fuse box.
IATF16949 Certified
The Bourns production facility for Multifuse® PPTC Resettable Fuses is certified to IATF16949. Together with ISO 9001:IATF16949 specifies the quality system requirements for the design, development, production, installation and servicing of automotive-related products.
AEC Certification
The Bourns® Multifuse® family of Polymeric Positive Temperature Coefficient Resettable Fuses can be certified to AEC-Q200-Rev D. This specification defines the stress test requirements and reference test conditions for qualification of passive electrical devices in automotive applications as defined by a committee of automotive companies.
RoHS Compliant*
All Bourns® Multifuse® Polymeric Positive Temperature Coefficient Resettable Fuses are RoHS compliant* as standard.