嘿!您似乎在 United States,您想使用我们的 English 网站吗?
Switch to English site
Skip to main content

Thingy:52146-3540)是Nordic Semiconductor的短程无线开发套件,旨在开箱即简化IoT功能和应用。该开发板基于nRF52832169-7118)系统芯片,该系统具有从蓝牙5.2NFCANT2.4GHz专有的一系列令人印象深刻的连接协议。Thingy:52最显著的特点称为IoT传感器套件”,即Nordic设法在如此小的地方安装了多少传感设备。该设备为套件提供了丰富的环境监控功能,包括温度、湿度、气压、空气质量、光的颜色,光的强度、运动和方向,所有这些都可以通过“Nordic Thingy”移动应用程序进行访问。 

Screenshot_%2810%29_244a64cbcaab9d81bf6cf9b010b1dcc324153e7f.png

Thingy:52硬件图 

本文的目的是演示“Nordic Thingy”应用程序提供的Thingy:52的即时功能,可以使用兼容NFC的智能手机扫描机箱顶部并点击链接转到应用商店找到并下载该应用程序。本文将使用安卓应用程序获取任何屏幕截图,但其他平台上的基本操作相同。 

设置和连接 

访问设备的功能就像打开设备一样简单。首先,这可能是一个挑战,因为开关被小心地隐藏在USB插座和JTAG端口旁边的橡胶保护盖下方。Thingy:52由内置的1440mAh内置锂电池供电,使该设备在无需额外硬件的情况下即可快速建立远程物联网功能,效率极高。该设备固有的低能耗架构还将确保电池更长的运行时间,充电就像连接微型USB电缆一样简单。给Thingy:52通电让智能手机应用程序可以在与任何无线功能进行交互之前通过蓝牙建立连接并配置设备。该应用程序处理这个过程非常高效,使用户可以快速访问开发套件所有有趣的部分。Screenshot_%2813%29_-_Copy_e536164579a70abcbf6a14f7dc0152a35b03c598.png

寻找隐藏的开关 

有趣的部分 

该应用程序将Thingy:52组织为五个功能选项卡,可以从屏幕侧面的拉出窗口控制和监视相关功能组。这些功能可以分为以下三个主要类别。 

 

Screenshot_20200821-132904_Nordic_Thingy_b34502181c406748c81fd90491659c899d976652.jpg

"Nordic Thingy" app侧边栏

感应 

Thingy:52广泛的感应功能可以通过应用程序的前三个选项卡进行访问。每个传感器的实时指标有助于实时量化即时环境数据,然后使用一系列动态线形图显示对其进行绘制。外推运动数据用于监视步进和轻点事件,而方向数据用于测量磁性轴承并以3D形式渲染设备的物理方向! 

Screenshot_20200819-164020_Nordic_Thingy_-_Copy1_7b31264ada6c347a0fd1ab69f870c9b1b0f296eb.jpg

 Thingy:52的传感器功能

串流 

Thingy:52带有集成的麦克风和扬声器,可以直接通过蓝牙串流音频。应用程序上的“声音”选项卡允许与设备进行半双工音频通信,从而使其可以用作短距离对讲机。对于更偏向于音乐的用户,“声音”选项卡上有单个八度音阶合成器、芯片调谐样本音板和许多PCM音频演示,听到这种音乐会让家庭成员感到困惑。 

Screenshot_20200825-205801_Nordic_Thingy_-_Copy_c5b2a8224483f15f5b186f3d411d6f34c73c3fba.jpg

 Thingy:52音乐功能

冲浪 

“云”选项卡让Thingy:52可以作为IFTTT客户端连接到更广泛的物联网领域,使其能够控制许多互联网功能(例如将动态数据发布到Twitter和类似的Webhook),这些功能允许该设备与其他硬件、应用程序和网站进行交互)。此功能使Thingy:52成为功能特别强大的物联网边缘设备,值得在以后的文章中进行进一步探讨。 

Screenshot_20200826-171545_Nordic_Thingy1_7ca8d0099e0c96db613d75604ce7d25e36cd7540.jpg

Thingy:52 Edge功能

结论 

Thingy:52是来自Nordic Semiconductor的出色物联网开发套件,它将丰富的环境感应功能与最新的蓝牙5标准结合在一起,创建了一个功能强大且易于使用的平台。专用的应用程序为开发人员的可访问性提供了一种全新的方法,该方法可以快速引入该技术,而无需编写任何代码。 

nRF52832芯片系统具有强大的中级ARM内核,使Thingy:52可以快速高效地处理传感器和网络数据。32位架构还通过连接低级数据与高级网关功能最大程度地提高设备的互操作性,例如蓝牙Webhook,使其成为功能出奇强大的物联网边缘设备。 

Nordic已经成功地将重点的物联网设计与用户友好的开发人员工具相结合,创建了一个令人印象深刻的硬件平台,非常适合潜在的物联网开发人员。nRF52芯片组通过集成最新的基于802.15的协议来确保其在快速扩展的物联网环境中的相关性,从而保证短距离无线应用的使用寿命。 

另外,如果您对蓝牙感兴趣,请参见蓝牙开发套件(146-3538)。 

A keen maker and electronic engineer with a passion for the environment, renewables, alternative transport and anything off-grid. Man with a van and founder of the Kickstart Kamper sustainable campervan project. Grassroots Education Sustainability Ambassador. BrightSpark 2017. BEng. KickstartKamper.co.uk