Skip to main content

4 reasons to use a fan speed controller in your application

With the continuous improvement in technology, every new product strives to achieve better performance than its predecessor, whilst maintaining a compact design. This is challenging the fan manufacturers in the electronics industry, as they now need to dissipate ever higher heat levels in the same space as before.

However, the desire of obtaining the highest performing option has always been in the customer’s mind, and therefore will always choose the highest performing fan he can accommodate in his enclosure.

Why use speed control then?

title

 

 

 

 

 

 

 

Typical chiller unit configuration

Flexibility

The fan selection is based on the extreme conditions the equipment might face, which means that if the fan does not have speed control it will be running at its maximum capacity 24/7. This can be detrimental, as the equipment will rarely be exposed to these extreme environments and hence the fan will be running above the duty required for most of the time.

With speed control, the fan can moderate its performance as required by the conditions making it more efficient and reducing the strain on the equipment.

Energy saving

Operating a fan further down the curve can have significant effects on its power consumption. This is clearly illustrated with the use of the fan laws.

According to the graph, a reduction of 25% in RPM will result in a saving of around 50% of the power consumption.

This is a theoretical value, and should only be used as an estimation.

However, it has been proven you can save up to 50% energy with only 22% speed reduction on many of our centrifugal blowers.

title

 

 

 

 

 

 

 

 

 

 

 

Figure 1: 3rd Fan Law

Noise

Noise is another important factor when it comes to speed control.

This is best seen when comparing an on/off operation with a speed control configuration in a multiple fan application.

According to the graph, a reduction of -15dBA can be achieved by operating all the fans at half speed, as opposed to the -3dBA reduction obtained by turning half of the fans off.

title

 

 

 

 

 

 

 

 

 

 

Figure 2: On/off operation vs Speed Control

Lifetime

Running the fans at their maximum operating speed will have an effect on their lifetime.

The bearing is the first component to fail in a fan under normal circumstances, and therefore the determining factor for this value.

With speed control the high temperature on the bearings are reduced, having a positive effect on the life expectancy.

There is test data showing that a 10% reduction in speed can double the lifetime of the product. 

EBMPAPST FAN CONTROLLER RANGE

Related Articles -  An intelligent way to control your cooling application – TMS

JJara has not written a bio yet…