How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Soldering nickel-plated copper with a highly active solder/flux can be challenging without
using the correct technique. While nickel-plated conductors offer excellent resistance to high
temperatures, it can be more difficult to solder than copper, silver, and tin. Nickel is commonly used at operating temperatures over 250° C and provides excellent corrosion resistance, but it requires a fully activated flux to limit oxidation at the high temperatures used during soldering.
Follow the Tech Tips in the attached document, it shows the correct soldering method for nickel-plated copper.
But first, Paige DiAntonio from Alpha Wire takes you through ThermoThin hook-up wire.
Released in 2017, Alpha Wire's latest advancement in wire technology arrived with ThermoThin hook-up wire. ThermoThin features an ECA fluoropolymer insulation and nickel-plated copper conductors. This particular family of wires features extreme temperature capabilities allowing it to reach temperatures as low as -150°C and as high as +300°C. In addition to the wide temperature range, ThermoThin wires are incredibly lightweight and thin making them versatile and suitable for a multitude of applications.
Having been on the market for over a year now, one challenge that has been identified by users has been the proper technique for soldering. Alpha Wire has provided the proper technique for soldering nickel-plated copper to better assist our customers.
For more information on ThermoThin, please visit the links below for the brochure, further technical questions, and to request a custom quote:
Brochure | Cable Expert | Custom Cable Quote
Follow Alpha Wire Today!
Twitter: https://twitter.com/alphawire
Facebook: https://www.facebook.com/Alpha-Wire-137296366311487/
LinkedIn: http://ow.ly/eNmW30eBlRB