DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
Bonjour,
Je n'arrive plus à faire pivoter ma pièce à l'aide de la molette de ma souris.
Quel paramètre a changé ou est-ce un problème de souris ?
D'avance merci
Patrick PARENT トラックの幅を大きくしすぎると,下のように表面実装部分を超えてしまうのですが隠す方法はありますか? Hello.
Decided to Try PCB Designer. The Registration Process obtained my information but, the link to the email verification produces a 500 Server Error. Upon trying to run the software, a pop-up shows "Invalid Credentials" when fetching the license.
Uninstall and re-install as Admin did not help.
Any ideas or suggestions?
Thanks
Ray
PS: Cross-posed in the membership/Website support forum.
I've been using DS v5 since it was originally released along with Solidworks Maker. I am looking to move to DS v6 Creator full time as it fits my purpose better, however, I am having an issue with saving drawing sheets. I have looked for tutorials but maybe it's too early yet since v6 just released. Maybe I am missing a setting or something. I get this message if I try to save the model or drawing. Any help with this is appreciated. Below is Error Message.
While I think the monthly subscription provides great flexibility for makers and others, I would really like the option to pay yearly (no cost reduction necessary). Hello, I'm new in DS and I've got simple problem, I can't save files to dxf? What should I do ? I read about space claims but its to v5.0 The button in the DSM6 help/resouces tab doesn't seem to do anything.
I think there is a kind of problem with STP:
there is no posibility to convert only chosen elements to STP
Converter processes everything regardless of whether it is active, marked or selected.
With STL I can chose and convert even one element - there is no such posibilities for STP converter.
完成後のオブジェクトのジオメトリを修正することができません。例えば、ブレンドしたオブジェクトを保存し、その後再度開いて、ブレンド前の各断面を修正したいのですが、その断面は再現されず修正できません。Blenderでは完成後もジオメトリ(点や辺)を修正することができますが、DSにも同様の機能があるのでしょうか。 Just downloaded the new version of DesignSpark Mechanical 6.0 and when i export to CURA nothing happens just the information show on the bottom of wuality and facets. Any help as to why it wouldnt export? Looking for some guidance on how to set up Home Assistant on a Rock.
Any guidance and input would be welcome.
https://www.home-assistant.io/
Can I continue to use my AddOn license (Export & Drawing) after updating from 5.0 to 6.0? Or do I have to update to Creator/Engineer?
Are there new features in Creator or Engineer that are not included in the AddOn package? Hello,
DS multilayer PCB vias have pads also in the layer with no connection. This implies that internal GND planes for example under a BGA have a lot of holes larger with respect to what needed for vias without unused pads.
Is there a way to avoid unused pads on vias?
Thanks
Antonio I've detected problem when trying load project file generated with DSM v5 to new DSM v6.
It's unable to load even simplest project file generated with DSM v5 to DSM v6.
Is this problem known?
When I try to load project file, I've got info message You can see as atachement.
You can see even 3D detail, but if I clik OK then loading stops.
Can You give me any helpfull info ? Just installed DSM 6.0
"Check for software update" button advises a new version: 6.0.4 is available from the subscription dashboard but it only shows the original DSM 6.0 download.
Where is it pls?最近のフォーラム投稿
Rotation
トラックの設定の仕方がわからない。
New Registration. 500 Server Error verifying email addr. Invalid Credentials
Drawing Sheets not Saving
Monthly Subscription
Can't save to dxf file
simulation upgrade?
How to convert only chosen elements to STP
完成後の修正方法
DSM6 Can not export to CURA
Anyone with experience running Home Assistant on Rock?
Updating from 5.0 to 6.0
unused pads of multilayer PCB vias
Failed to load body geometry when trying load project file generated with DSM v5 to new DSM v6.
Can't find 6.0.4 update