- Startseite
- Community
- Foren
DesignSpark Foren
Kommunizieren Sie über den Forenbereich frei mit anderen Mitgliedern von DesignSpark. Eröffnen Sie neue Unterhaltungen oder beteiligen Sie sich an bestehenden Diskussionen über Produkte, Technologie, Software und zukünftige Neuheiten. Helfen Sie mit, Lösungen zu finden oder suchen Sie nach Antworten auf Ihre eigenen technischen Probleme, indem Sie auf ein globales Netzwerk von gleichgesinnten Ingenieuren zurückgreifen.
kann die V6 nicht installieren (keine altere Version vorhanden). Bricht mit Fehlercode 2503 und 2502 ab.
hi
I installed ver.11 and works fine.
I'd like to know adds and differences compared to the old versions.
Is there a link somewhere to read them ?
many thanks
I am in despair, I cannot get this unusual object out of the drawing. In maplist I have 20 items that is 20 videos I want to do is play video which comes in center of viewport and pause all others and keep that behaviour throughout scrolling:
const [reels, setReels] = useState([]);
useEffect(() => {
fetchAllVideos();
}, []);
const fetchAllVideos = async () => {
const getAllVideosRes = await getAllVideos(pageNumber);
setReels(getAllVideosRes);
};
return (
<>
reels.map((item, idx) => {
return (
<MDBox mb={3} key={idx}>
<Card sx={{ borderRadius: "25px" }}>
<video style={{ height: "100%", width: "100%", objectFit: "cover", borderRadius: "25px", }} loop controls>
<source src={item.photo} type="video/mp4" />
</video>
</MDBox>
</Card>
</MDBox >
);
})
</>
) Bonjour,
Je n'arrive plus à faire pivoter ma pièce à l'aide de la molette de ma souris.
Quel paramètre a changé ou est-ce un problème de souris ?
D'avance merci
Patrick PARENT トラックの幅を大きくしすぎると,下のように表面実装部分を超えてしまうのですが隠す方法はありますか? Hello.
Decided to Try PCB Designer. The Registration Process obtained my information but, the link to the email verification produces a 500 Server Error. Upon trying to run the software, a pop-up shows "Invalid Credentials" when fetching the license.
Uninstall and re-install as Admin did not help.
Any ideas or suggestions?
Thanks
Ray
PS: Cross-posed in the membership/Website support forum.
I've been using DS v5 since it was originally released along with Solidworks Maker. I am looking to move to DS v6 Creator full time as it fits my purpose better, however, I am having an issue with saving drawing sheets. I have looked for tutorials but maybe it's too early yet since v6 just released. Maybe I am missing a setting or something. I get this message if I try to save the model or drawing. Any help with this is appreciated. Below is Error Message.
While I think the monthly subscription provides great flexibility for makers and others, I would really like the option to pay yearly (no cost reduction necessary). Hello, I'm new in DS and I've got simple problem, I can't save files to dxf? What should I do ? I read about space claims but its to v5.0 The button in the DSM6 help/resouces tab doesn't seem to do anything.
I think there is a kind of problem with STP:
there is no posibility to convert only chosen elements to STP
Converter processes everything regardless of whether it is active, marked or selected.
With STL I can chose and convert even one element - there is no such posibilities for STP converter.
完成後のオブジェクトのジオメトリを修正することができません。例えば、ブレンドしたオブジェクトを保存し、その後再度開いて、ブレンド前の各断面を修正したいのですが、その断面は再現されず修正できません。Blenderでは完成後もジオメトリ(点や辺)を修正することができますが、DSにも同様の機能があるのでしょうか。 Just downloaded the new version of DesignSpark Mechanical 6.0 and when i export to CURA nothing happens just the information show on the bottom of wuality and facets. Any help as to why it wouldnt export? Looking for some guidance on how to set up Home Assistant on a Rock.
Any guidance and input would be welcome.
https://www.home-assistant.io/
Neue Forumsbeiträge
Installation Fehlermeldung 2503 und 2502
news and add on ver. 11
Unwanted object cannot be removed from the drawing.
ReactJS: How to play video which comes in center and pause all other videos
Rotation
トラックの設定の仕方がわからない。
New Registration. 500 Server Error verifying email addr. Invalid Credentials
Drawing Sheets not Saving
Monthly Subscription
Can't save to dxf file
simulation upgrade?
How to convert only chosen elements to STP
完成後の修正方法
DSM6 Can not export to CURA
Anyone with experience running Home Assistant on Rock?
Unser Forum
Software
Community
Ambitionen als Ingenieur
- Beiträge
- 2
Mein erstes Design-Projekt war
- Beiträge
- 16