Sponsored by: NVIDIA
2025: The Year of Arm Chips and AI-Powered PCs
2025 is shaping up to be a pivotal year for Arm architecture, with significant developments across both cloud and consumer computing. As Arm-based systems continue to gain momentum, two key initiatives stand out: GitHub’s introduction of Arm-hosted runners for streamlined application development, and the highly anticipated release of NVIDIA and MediaTek’s AI PC system-on-chip (SoC).
GitHub Embraces Arm Architecture for CI/CD Workflows
GitHub, with over 100 million developers on its platform, has recently launched Arm-hosted runners for GitHub Actions, a move that could redefine how developers build and deploy applications. Previously, developers had to manage their infrastructure or use slow emulation for Arm-based applications. With the new Arm-native runners powered by Arm Neoverse, developers can now enjoy native performance, improved energy efficiency, and reduced costs for their workflows.
These hosted runners enable developers to build applications for various sectors, including automotive, cloud-native, and AI, all while benefiting from GitHub’s familiar CI/CD environment. Key advantages include:
- Native Performance: Running build and test cycles directly on Arm processors eliminates the need for cross-compilation and emulation, significantly improving efficiency.
- Cost and Sustainability: Arm’s architecture is known for its power efficiency, with GitHub estimating that Arm-based servers use 30-40% less power than traditional x86 servers. This reduces operational costs and the carbon footprint of development processes.
- Broader Use Cases: Arm-native runners open new possibilities for developers working on multi-architecture applications, automotive software, and edge AI applications, especially with frameworks like PyTorch and llama.cpp optimized for Arm.
The GitHub and Arm collaboration signals a broader industry shift toward Arm-powered computing, reflecting the growing importance of sustainability and cost-effectiveness in cloud computing and software development.
NVIDIA and MediaTek's AI PC SoC: A Game-Changer for the PC Market
In the consumer hardware space, NVIDIA and MediaTek are set to release an AI PC SoC in the second half of 2025, which could potentially disrupt the PC industry dominated by Intel, AMD, and Qualcomm. The SoC, which will be built on TSMC’s 3nm process and based on Arm architecture, is expected to deliver significant advancements in AI-driven computing for personal computers.
NVIDIA’s expertise in AI and graphical capabilities, combined with MediaTek’s prowess in mobile chip development, makes this partnership one to watch closely. The AI PC SoC is designed to handle cutting-edge AI workloads, positioning it as a powerful alternative to conventional x86-based CPUs. Major OEMs like Lenovo, Dell, HP, and ASUS have already expressed interest, signalling strong market adoption upon release.
While details about the specific features remain scarce, the chip is expected to integrate NVIDIA’s next-gen iGPU, pushing performance standards to new heights. This collaboration underscores a broader trend where AI is becoming a central component in consumer and enterprise computing, a trend NVIDIA and MediaTek aim to lead.
The Rise of Arm in 2025
Both GitHub’s Arm-hosted runners and NVIDIA’s AI PC SoC represent milestones in the broader adoption of Arm architecture across industries. Arm’s power-efficient, scalable, and versatile architecture is increasingly being leveraged for cloud-native applications, edge AI, automotive, and even personal computing. As Arm continues to expand its influence, 2025 could mark the year when the architecture solidifies its place as a dominant force in both development and consumer technology.
Whether it’s through the efficiency gains seen with GitHub Actions or the revolutionary impact of NVIDIA and MediaTek’s AI PC chip, Arm is set to play a critical role in shaping the future of computing. With enhanced CI/CD workflows for developers and powerful AI-driven hardware for consumers, 2025 may well be remembered as the "Year of Arm."
Source:
Comments