Dave from DesignSpark
Que pensez-vous de cet article ? Aidez-nous à vous fournir un meilleur contenu.
Dave from DesignSpark
Merci! Vos commentaires ont été reçus.
Dave from DesignSpark
There was a problem submitting your feedback, please try again later.
Dave from DesignSpark
Que pensez-vous de cet article ?
Spark erosion enables the machining of even very hard metals with almost no forces being transferred to the workpiece or to the CNC machine. This means that metals can be machined even with the mechanics of a 3D printer.
Parts list
Qty | Produit | Part number | |
---|---|---|---|
1 | RS PRO, 36.88 W, 12 V dc, 82.08 gcm, 4289 rpm, 6.35mm Shaft Diameter | 321-3186 | |
By using a DC motor (321-3186) as a "Wagner's hammer", a steel disc can be engraved. The motor is switched in such a way that the electrical circuit is closed via the workpiece. The motor must be polarized so that the electrode is then raised. If the circuit is interrupted again, the electrode is moved back to the workpiece surface via a spring.
The electrode "hammers" on the workpiece, the sparks created when the circuit opens, erode the metal. A video shows the process:
The graphic engraved with this system is only 15x16mm small, the digit height of the timestamp on the back is only 2.2mm: