How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Mike Meakin has created a "Hacksheet" explaining how to hook up your eRIC modules.
This is to be read in conjunction with the eRIC module datasheets and the eRIC Breakout Board datasheets.
The Break Out Board design is ‘Open Hardware’ and is designed and published by: Rick Winscot – www.quilix.com
See: https://github.com/rwinscot/eRIC-breakout
Mike's Hacksheet oulines how easy "hooking up" eRIC RF modules is, "...Using an eRIC Breakout Board (BoB) the surface mount castellated eRIC connections are brought out to more convenient 0.1" pitch pins that can be plugged into any prototyping breadboard."
"Power and logic level serial input and serial output are the minimal connections required. Serial data is ‘inverted’ allowing direct connection to uController UARTs or connection to PC serial ports via level shifter/inverters."
"A USB to logic level converter (Arduino FTDI Basic or Friend or similar) can alternatively be used if full
‘handshaking’ is required. Use of handshake (flow control) is optional but should be used for highest data throughput."
"eRIC operates on a 3.3V supply. Take care not to damage inputs when connecting to any 5V powered devices by fitting 1k resistors in series with the signal lines as shown in the diagrams. eRIC outputs should be able to drive 5V logic level inputs or loads sinking or sourcing no more than 10mA such as LEDs etc. The power supply should be locally decoupled and capable of continuously supplying the peak transmit current."
"Low power modes are set using serial commands detailed in the eRIC data sheet."
"Between 1 and 250 bytes of data can be sent in one transmission which automatically begins when the buffer is full or when ‘no data’ is detected for twice the character time. Over air data rate is 38400 bps. Host data rate can be set between 2400 and 115200 Baud (19,200 default)."
"A ¼ wave whip antenna can be connected directly to the on board SMA RF connector or via a flexible 50R cable to the eRIC UFL connector."
For Technical Support see: www.lprs.co.uk/resource-centre/support/