How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Hardware test for DC DC interleaved boost converter
Hardware test for Monolithic interleaved boost converter with MPPT:
-Hardware model: ST microelectronics, ISV008V1, (complementary 3 X SPV 1020)
-Use DC power supply and photovoltaic cell 2V to 28V input voltage
-Value and waveform of V, I, P, I ripple will be recorded by CRO.
PSIM simulation will be repeated if true hardware parameters are obtained by manufacturer’s manual or measurement.
Previous PSIM simulation data:
The ISV008V1 has 3 sets of SPV1020 on same board and could be operated separately. DC power supply is used for hardware test and use only one channel for safe.
Rheostat is adopted as a resistive load for adjustment.
It is found that ISV008V1 requires an initial voltage for its operation. The gain is around 4~5 times and similar to the PSIM simulation.
The data are measured from one of the channel of ISV008V1. The converter will be operated when input voltage ranges around 6V~10V in two resistive loads.
The input voltage is about 8V and the converter will not further boost the output voltage though that rises to 18V.